This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC21530: High Side Gate Driver Outputs 1/2 VDDA

Part Number: UCC21530


I am using the UCC21530DWKR to drive a Full-Bridge Converter. I am using 24V-to-15V isolated DC-DC converters to power the VDDA and VDDB respectively. When I ramp up the bus voltage to approximately 200VDC for the Full-Bridge converter, the high side driver of the UCC21530 begins to output at 1/2 of the VDDA. After moments of this occurrence, the output of the high side gate driver fails short to the VSSA. Is this a common issue or has this been seen in other applications.