Dear TI,
I am using LM5116 Power management IC for dual output interleaved buck converter for around 12V/50A application. I have battery at output side and load as well. I want to enable the controller when battery is connected at the output side until unless controller should not enable.To achieve this i was terminated the input supply pin number 01 and supplied the VCCx from battery. In this scenario, some 8V is appearing at the output without connecting Battery. From where this internal regulator getting supply.?