Other Parts Discussed in Thread: BQ78350
Hello Sir,
I'm working on 76940 EVM that comes with a BQ78350 battery monitor chipset.
While using the BQ78350 for charging my 15S1P pack with a nominal capacity being 2.2Ah and charging current
set at 0.6 A what I'm observing is the charging current is not restricted by the battery monitor meaning. Even if
the source provides a current of 2A to the battery pack the pack charges with 2A when actually the charging current
set in the fast charging algorithm is just 0.6 A what could be the issue or the setting that can resolve this issue
Regards
MIHIR