This is a general question regarding which approach is better. With a 2-level, 3 phase inverter with a connected load and the IGBT drivers enabled.
Could i know which of the following 2 options is better. The DC link voltage can be up to around 350V
1) Apply the gate signals to the drivers, wait a second or so, then turn on the DC link voltage to the IGBTs .
OR
2) Apply low level signals to the IGBT drivers ( i.e low gate drives to the IGBTs) then apply the DC link voltage , wait a second or two then start applying the
correct gate triggering sequence to generate the desired IGBT gate triggering.
Thanks