Other Parts Discussed in Thread: TPS61196
Hi,Sir:
Could you kindly help to check whether the TPS61169 had minimum duty cycle and dimming on time spec?
for example, even the minimum duty is 1% and PWM dimming frequency is 100KHz with 1 serial led(20mA),
that means a 0.1uS dimming on time with 1 serial led(20mA),
as the TPS61169 could be work well and the LCD's backlight function also be good?
Thanks!