Other Parts Discussed in Thread: BQ76PL455A-Q1, , BQ76PL455A
In the bq76PL455A-Q1 datasheet https://www.ti.com/lit/ds/symlink/bq76pl455a-q1.pdf?ts=1596059302879&ref_url=https%253A%252F%252Fwww.google.com%252F it is stated on page 1 that the maximum number of bq76PL455A-Q1 connected in series via the daisy-chain is 16. So that would give you a maximum total battery voltage of 4,2*16*16 = 1075V which would be achievable with this IC.
But in the user guide for the bq76PL455EVM evaluation module https://www.ti.com/lit/ug/sluuba7a/sluuba7a.pdf?ts=1596059608499&ref_url=https%253A%252F%252Fwww.ti.com%252Ftool%252FBQ76PL455EVM%253Futm_source%253Dgoogle%2526utm_medium%253Dcpc%2526utm_campaign%253Dapp-null-null-GPN_EN_EVM-cpc-evm-google-wwe%2526utm_content%253DBQ76PL455EVM%2526ds_k%253DBQ76PL455EVM%2526DCM%253Dyes%2526gclid%253DEAIaIQobChMIosKvqLnz6gIVVeDtCh0LrgisEAAYASAAEgIQ0_D_BwE%2526gclsrc%253Daw.ds it is stated on page 3:
“For battery stacks with more than 16 cells, stack up to 6 bq76PL455EVMs in series to support up to 96 cells. Communication with stacked bq76PL455EVMs is via an isolated daisy-chain differential bus capable of withstanding 500 V.”
So do I assume correctly that this limitation is board specific because of the isolation limit of the daisy-chain differential bus on the evaluation module? Would it therefore be possible to connect more than 6 bq76PL455EVM in series if I would for example use LiFePO4 cells with a maximum cell voltage of 3,6V? In this case for example 8 bq76PL455EVM with a maximum total voltage of 8*16*3,6 = 461V < 500V?
Thank you in advance for your answer!
Best regards,
Joachim