This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP38512: LP38512 delay

Part Number: LP38512

Hi Sir,

Pls kindly reference as below customer schematic.

O/P will have 6ms delay after EN, what will possible cause it?

Thanks, Ian.

  • Hi Ian,

    This is likely do to the propagation delay from the EN pin going high to the output rising. 6us is actually much faster than what is shown in the datasheet:

    Does this answer your question?

  • Hi Guys,

    But customer delay is "6ms", it's really slow than d/s.

    Thanks, Ian.

  • Hi Ian,

    Can they measure the voltage at the Enable Pin, VOUT, and the load current?

    Thanks,

  • Hi John,

    Yes,  

    Blue channel “En” is Enable Pin.

     Green channel “3.3V_CIS” is VOUT.

    Red channel “Current” is the load current.

    Thanks, Ian.

  • Hi Ian,

    It will have to confirm with design, but it looks like this part has an internal charge pump. If is not shown in the block diagram nor described in the datasheet, but the block diagram shows that the device is using a NMOS as the pass element:

    To support a VDO of <=400mV, there must a charge pump for the internal gate bias supply. It could be that the reason the plot in the PDS showing a faster startup from just the EN pin vs VIN and the EN pin could be that the charge pump needs to startup and raise the internal bias rails to properly modulate the gate of the NMOS.

    Does this help to clarify? Also, it looks like the current limit is being hit during startup. How much capacitance is at COUT?