Part Number: UCC37321
Other Parts Discussed in Thread: UCC37322,
around 2 or 3 months ago, I ordered 5 sets of ucc37321 and ucc37322, and around 1 week ago I got the time to use it in a project, but when I powered the project on, the ucc37321 ic keeps dying after 3-5 seconds or so, but the ucc37322 ic didn't, both of the ic was used to drive a gate drive transformer that should drive a half-bridge, I don't understand what happened then because the ic keeps dying and shorting after 3 attempts of ic replacement .the Vin for the ic was 12v and it was drawing around 600-800mA when it was working in the first 2 seconds. is it a problem with my circuit ? also I realized when the ic was working, I was probing the output of the ic and there was a 1.4Mhz oscillation when the ic was working, is it the ringing problem? since I only have 1 more ic again, I can't trust my circuit, since ordering one could take ages.. also I will attach the gate driving circuitry in here, thank you...
the full circuit can be found on http://stevehv.4hv.org/SSTC5/miniSSTCsch.JPG