My customer is looking for a buck controller for the below application. Since the system is naturally cooling, so they prefer controller and external mosfets.Could you please help suggest it? Thank you.
1) Working temp. -5~ 125C.
2) 12Vin, 5V output, 80W.
3) Efficiency > 97%
4) Non-isolated.
5) Current loop or forward feedback is preferred to address the input disturb.