This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5045: The value of SS cap and Rd resister

Part Number: LM5045

Hi Expert.

Ioperating the LM5045 open loop, with no feedback.

I have 2 questions.

Q1.I have heard that the recommended range of the SS cap is 0.1uF to 1uF .

    I change  SS cap is  1uF.But  inrush current is large,(inrush current is peak 10A)

    I  want to suppress. Could I set  a higher value? (ex. 2.2uF)

Q2. I operate LM5045 open loop, with no feedback. I think secoundary dead time is 0sec.

    Could I set Rd resister is 0Ω?