Part Number: BQ25570
Hi,
I’m interested in using the BQ25570 to charge a lipo cell. I have a low power MCU which will work fine off the buck converter. However, I also have a radio with a pulse current of ~500mA or so. Is it possible to run the radio directly connected to the battery while the BQ25570 is operating? Radio transmissions are rare, but they will happen.
Thanks.