This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25713EVM-017: BQSTUDIO SUPPORT and DOA

Part Number: BQ25713EVM-017
Other Parts Discussed in Thread: BQ25713, BQSTUDIO, EV2400

Hi Team, 

A customer of mine who is evaluating the BQ25713EVM-017 had the following observation: 

The BQ25713 seems to be DOA, when we connect 5V to the input, the power LED blinks.

It is constant only at higher voltages  (while this board should be able to work with voltages <5V).

Furthermore we don't get communication via BQstudio. We connected the BQ25713 to an EV2400 via SMBUS but get an ACK error on all commands.

Can you please advise how they could resolve these issues? 

Thanks. 

Obinna.