This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5069: LM5069 or TPS2493, which one is the best fit for our Hotswap application?

Part Number: LM5069
Other Parts Discussed in Thread: TPS2493, TPS1663

Hi Expert, 

We are desiging 48V power supply system. Becuase the backed DC/DC is using nonisolated solution, so the hot swap protection is very important. The current requirement is no more than 4A.  Checking the TI series, the LM5069 and TPS2493 are good candidates with similar features. The good of LM5069 is small package, the good of TPS2493 is that it's relatively new generation. From reliability point of view, which one is best fit? We prefer LM5069 because it's small, but reliability is key factor.

Thanks

Peter