Part Number: LP87564-Q1
Hi team,
Is that possible to separate VIN_Bx for each buck?
For example VIN_B1 connect 5.0V and VIN_B2 connect 3.3V.
I would like to use this device as independent 4 converters.
regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LP87564-Q1
Hi team,
Is that possible to separate VIN_Bx for each buck?
For example VIN_B1 connect 5.0V and VIN_B2 connect 3.3V.
I would like to use this device as independent 4 converters.
regards,
Shinji Tsuji,
I have assigned this question to the experts on the device, but they are in Europe and it is after 5pm local time so you may not receive a reply until tomorrow.
Hello,
Unfortunately it is not possible. All bucks must have the same VIN and also the VANA must be connected to the same rail.
Thansk.
Regards
Tomi Koskela