This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD3138PSFBEVM-027: UCD3138-PSFB-EVM27 source code difference

Part Number: UCD3138PSFBEVM-027



Hello.

I just bought a UCD3138-PSFB-EVM27. I tested it and found that its waveform is consistent with the user manual. For example, the output voltage has no overshoot during startup and the no-load loss is about 32W.

Later, I downloaded the source code from the official website and re-burned it into the development board. I found that the output voltage will overshoot when it starts, and the no-load loss is about 17W.

I think there is a difference between the source code published on the official website and the source code actually burned by the development board.

Please also send me the final source code burned by the development board. Thank you. Email: zouyang90@163.com