Hi,
I have two questions of TPS61178
1. What is this IC DUTY MAX & DUTY MIN?
2. When 12.5V boost to 13V, the DUTY is about 4%, can this IC be used in such a low DUTY range? Whether it is over design in the actual application of the IC?
The SPEC as the follow
|
Vin(min) |
7V |
|
Vin(max) |
12.5V |
|
Vout |
13V |
|
Iout |
3A |
Thanks and best regards
Rock Shao