Other Parts Discussed in Thread: LM62440-Q1, , LM60440-Q1
Hi,
For telematics project I need a DCDC Converter from 12V battery down to 5Vout @4A.
Vin_max 21V.
I was looking at LM60440-Q1 but I cannot tolerate EN= Vin +- 0.3V as Enable pin can have variations much more than +-0.3V than Vin. So I was considering LM61440-Q1 or LM62440-Q1.
Do these 2 p/n avoid the issue with EN pin I have with LM60440-Q1?
What are the differences among LM61440-Q1 and LM62440-Q1? The ds seem to be the same but price is different.
Many Thanks,
Antonio