Hi Team,
Here are several questions on TPS63070.
1. Vout=3.52V, L=1uH, Cout=80uf ( derating is 50%).
When Vin is ~3.52V, output ripple becomes much larger than the condition that Vin is smaller or larger. Is it normal? To my understanding, maybe it changes between buck and boost, so the ripple is larger.
2. To decrease ripple, increase L to 2.2uH.
When Vin is 3.7V, output ripple becomes much larger. what's the reason for this that Vin-Vout changes with inductor?
3. In datasheet, it mentioned when inductor is increased, you need to increase Cout. And it is related with RHPZ of boost and need more Cout to decrease the cross over frequency, could you please kindly provide more details?
Thanks.
BRs
Given