This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/TPS568230: Burnout of the TI Buck Regulator on the TI RSLK MAX chassis board

Part Number: TPS568230

Tool/software: WEBENCH® Design Tools

When the chassis board for the TI RSLK MAX, is used with 6 Alkaline batteries instead of the 6 NiMH batteries the TI Buck Regulator TPS568230 burned out. There was smoke and high heat produced on the chassis board after the device was turned on. Could you share the reason why behind this? I thought the regulator could handle a load of about 4.5 V Min and 12 V max but the alkaline batteries summed up to 9 V only.