Other Parts Discussed in Thread: TPS53515, TPS54824
Hi Expert,
A TPS62180 is used to convert 12V to 5.55V.
A few PCBA were fabricated at different time against the same schematic diagram, the same PCB layout and the same peripheral components. However, only the PCBA made at the 1st time succeeds. It converts the voltage with an input power of 22.2W at an efficient of 91%。
The rest PCBA either cannot deliver 3.6A, or work at a low efficiency of 63%.
The only schematic diagram is display below.
The only PCB Layout is shown below.
The same PCBA is here
Do you have any clue which results the circuit deficiency? Or, do you have any suggestion on circuit debug?
Thank you in advance!
Wallace