Other Parts Discussed in Thread: TIDA-01393
Hi support team,
I have three questions about "SLVUBK0B".
TPS65086100 User's Guide for NXP LS1043A
www.ti.com/.../slvubk0b.pdf
(Q1)
Is the following voltage output when the VSYS pin becomes +5.6V or more?
LDO5P0(56pin)+5V / 100mA(TYP)
LDO3P3(54pin)+3.3V / 40mA(MAX)
LDOA1(9pin)+3.3V / 200mA(MAX)
(Q2)
Can the power outputs of (Q1) be used as a standby power supply for controlling the "CTL1 signal"?
(Q3)
Can I pull up the DATA, CLK, GPOx and CTLx signals by "LDO3P3 (54pin) +3.3V"?
Regards,
Dice-K