Other Parts Discussed in Thread: TPS56637
Hi team,
I installed SPICE for TI 2020 and TPS56637 PSPICE transient model on Ti.com.
I added DC 15 V as an input and R10(20 kΩ),C7(100pF) in Feedback area surrounded by a red frame in the picture
and put probe on Vout, and configured Simulation setting.
I also set the value of "Run to Time": to 3.5 ms and Maximum Step Size to 0.1 ms.
Atfer I push "RUN", I could not get results of the simulation but PSPICE for TI 2020 freezes.
How can I fix this error?
Best Regards,
Maki