This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24298: Undefined current regulation

Part Number: BQ24298
Other Parts Discussed in Thread: BQ24296M
When I use the ic with default settings for charge current limit and with an adapter that can offer curretn up to 3A the current limit should be at about 2A. But if I replug the power connecter several times, it sometimes enters a state where it is charging with around 640mA.
This only happens when the watchdog of the bq2498 ist triggered to stay in host mode
If i replug the power connecter again it always charges with ca 640mA unless i unplug it and wait for the 40s to cause a watchdog reset of the controller