This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50: FCC error

Part Number: BQ40Z50

Hello TI members

Currently our device which utilize BQ40z50(FW version R3) has an FCC error greater than 2% criteria. 

Our pack supplier is working on Rb tweak to fix the issue. 

My question is, will the slight FCC error (2~3%)  impact the Available Battery Life calculation? 

ABL is define as the time it takes for system to consume battery capacity from 100% to 5% RSOC, considering RSOC accuracy test passed.

Thank you for the support 

Best Regard, Patrick