This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS544B20: The default value of the IOUT_OC_WARN_LIMIT

Part Number: TPS544B20

Hi Experts,

I would like to understand default setting of IOUT_OC_WARN_LIMIT.  Which one is the default value? As you can see below table, it is stated three values. I think F828h(20A) is right one. Is it right? According to the datasheet p38, IOUT_OC_WARN_IMIT is calculated by Mantissa divided two. So 28h(HEX) is 40(DEC), then 40(DEC)/2=20A. Is my understanding correct?

Best Regards,
Fujiwara