Hi,
Let me discuss the OVP mode of TPS25924.
In that evaluation, μsec order ringing is applied to VIN.
I want to know if it is in OVP mode due to this input/output difference.
・Vin:12V ・Iout:≒2A ・Ringing peak voltage: 18V/1μsec
1.Could you tell me the detection time and threshold of OVP mode.
2. Related to question 1, how long does the TPS25924 exceed 10W for thermal foldback control?
And Could tell me the detailed operation of thermal foldback and the method to confirm whether or not the thermal shutdown has occurred.
I would like to know the input/output voltage/current waveform and diagram of thermal foldback operation.
I would like to send you a private message about the actual waveform and schematic.
Best regards,
Yusuke