This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS57160-Q1: TPS57160-Q1

Part Number: TPS57160-Q1

Hi team,

In the datasheet,Equation 47 (Pg35) and equation 51(Pg36), how can we find the value of gm(ps) and gm(EV) to calculate?

on page 5, 7.5 Electrical Characteristics,Which value is gm(ps) or gm(EV)?

Another question,about example application in the datasheet.

on page 35,It says"The example application is using a low ESR ceramic capacitor with 10 mΩ of ESR making the zero at 338 kHz."

on page 31,It says"Additional capacitance de-ratings for aging, temperature, and dc bias should be factored in, which increases this minimum value. For this example, a 47-μF 6.3-V X7R ceramic capacitor with 5-mΩ ESR is used."

Is the Esr of  Cout  5-mΩ or 10-mΩ in the example application?thank you.