Other Parts Discussed in Thread: BQ40Z50-R1, BQ40Z80
Hi ,
I have some questions that described as below:
1. What is CEDV?
2. Does BQ78350-R1 need to accompany AFE? Why? What is its difference between it and other gauge?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi ,
I have some questions that described as below:
1. What is CEDV?
2. Does BQ78350-R1 need to accompany AFE? Why? What is its difference between it and other gauge?
hi Miles,
1. Please find more info on CEDV vs. IT on this previous E2E post
2. As per the section 8.1 of the BQ78350-R1 datasheet: "
The bq78350-R1 Li-Ion and LiFePO4 Battery Management Controller is the companion to the bq769x0 family of Analog Front End (AFE) protection devices. This chipset supports 3-series to 15-series cell applications with capacities up to 320 Ah, and is suitable for a wide range of portable or stationary battery applications. The bq78350-R1 device provides an accurate fuel gauge and state-of-health (SoH) monitor, as well as the cell balancing algorithm and a full range of voltage-, current-, and temperature-based protection features."
HI David,
Good to receive your reply. As you says, the bq78350-R1 device can act as state-of-health (SoH) monitor, so it should not need AFE anymore. Am I right?
Miles,
If you look at a gauge like BQ40z50-R1 or BQ40z80, they are gauges which integrate the AFE.
BQ78350-R1 doesn't integrate the AFE and requires the V / I / T data measured by the BQ769x0 AFE to calculate & report the SOC / SOH...