Other Parts Discussed in Thread: BQ78Z100, , BQ28Z610
Hi,
Is the HDQ interface feature of the BQ78Z100 the only difference between these two devices? If I only need the I2C Interface which device is recommended?
Regards,
Patrick
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Is the HDQ interface feature of the BQ78Z100 the only difference between these two devices? If I only need the I2C Interface which device is recommended?
Regards,
Patrick
Hi Kang Kang,
Thank you for your reply. I did compare the TRMs and could find the following differences:
BQ28Z610-R1 has the following additional main features:
- BROADCAST mode
- Battery Trip Point (BTP) Interrupts
- Emergency FET Shutdown
- Voltage Imbalance
- Update version of State-of-Health
There are some more small differences between these two devices.
Regards,
Patrick