Hi Experts,
- Our company is going to program the UCD3138 before SMD. After mounting on the main board, there is a DIP process.
- Will UCD3138 lose its programmed data because of heat? (About 280 Celsius degree, 6 seconds)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Experts,
- Our company is going to program the UCD3138 before SMD. After mounting on the main board, there is a DIP process.
- Will UCD3138 lose its programmed data because of heat? (About 280 Celsius degree, 6 seconds)
the Operating Temperature for UCD3138 is: –40°C to 125°C
the absolute maximum junction temperature is : –40°C to 150°C
Hi Bosheng,
- Did you mean that over 150°C will cause UCD3138 broken?
- Is there anything related to temperature that will cause data lose? (PFlash and DFlash)
Jack, Over 150C may cause may cause permanent damage to the device and data lose.