Part Number: UCC28710
Other Parts Discussed in Thread: UCC28700
Hello,
I desinged a Flyback with a multi-output windings transformer. There are fours outputs: two 24v, one 12v and one auxiliary 17v to supply the controller.
In the experiment, my problem occurs when the output 12v is charged up to 2A during 40ms. After this time, the controller enters in an operating mode with its minimum switching frequency of 700Hz. This operating
mode lasts about 30ms and the controller gets out of this mode and goes back to its previous operating mode. It is quite same as "burst mode".
Do you know about this operating mode or have same phenomena like mine?
Looking forward to getting many feedback :).