Hello,
I would like to ask for technical support on my test setup for the leakage current into the PG pin of the device.
I always get the values of around 1uA , which is already outside the guaranteed maximum IPG,LKG of the device.
Here is how I did it:
1. Supply 3.3V on VBIAS pin
2. Force 0V on VOUT pin
3. Force 3.3V on VIN pin
4. Force 1.2V on ON pin (enable switch)
5. Then Force 5V on PG pin, and measure current
* CT and PG pins have no connection
Is this a correct and valid setup? And how is testing an output pin current leakage different from an input leakage test?
Thank you for all your help.
Regards,
Abraham