Hi,
I'm using a webench suggested schematic for a boost circuit (please see attached PDF design report) operating on a 24v input and boosting to 36V. During trouble shooting, i scoped the RC pin which correctly shows a sawtooth waveform within 245khz. However on scoping the gate pin of the mosfet i could find the gate voltage to be a little more than just 2 v which seems quite a bit odd to me. The FET I'm using is PSMN017-60YS from Nexperia which I had and is almost equivalent to the suggested CSD18543.
The attached scope shot is of the gate pin.
Any pointers to getting this working is highly appreciated.
Thank you
TPS40210-DER_36v_5A.pdf