This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62152: POwer off time

Part Number: TPS62152


Hi,

Kindly let me know the time(Off time) from enable to output when enable is low(Output also low) of TPS62152RGTR

Warm regards,

Monisha OM

  • Monisha OM,

    After consulting with the internal engineering team, the internal circuit will disable the output switching within a  couple microseconds of the EN falling below the disable threshold (0.45V).

    Please note that as there is no active discharge on this device, the output voltage will be discharged by the external load and through the feedback voltage divider network.  Additionally, as the PG pull down is asserted when EN = Low,  if you have a resistor between PG and Vo, the output voltage can be  discharge through this path as well.

    Thank you,

    -Matt