Other Parts Discussed in Thread: BQSTUDIO, BQ40Z80
I want to do a learning cycle with my hardware and pack, but I saw that the current readings are off. There is a both an offset (-30 to -40 mA reported with no load or supply attached), and some sort of error (it doesn't scale correctly as I adjust the current.
I can run the calibration through bqStudio and get it to report the correct value at a given point, but it isn't accurate at other current points (and it still ends up an offset of 30-40 mA). What am I missing? Thanks!