Hi, the attachment file is an application relative to tps23754 which we used for the very first time,could you help review this application please,thx.
looking forward for your kindly reply.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, the attachment file is an application relative to tps23754 which we used for the very first time,could you help review this application please,thx.
looking forward for your kindly reply.
Hi Jane,
This is currently being looked into. A response will be posted when available. Please note we are currently heavy on apps support so the initial review may be delayed at most by Wednesday. Please let us know if this is reasonable on your side. Thanks!
Hello,
Here are my comments:
- C2153 should be 0.047uF.
- It appears that there are only ceramic caps for the board. It would be best if the input caps, the VC cap and the output caps where electrolytic as the TPS23754EVM-383 is
-Otherwise, it appears to be exactly the same as the EVM. Can you confirm?
If this post answers your question, please indicate so by marking this thread as resolved. Thank you.
Regards,
Michael P.
Applications Engineer
Texas Instruments
Hello, I have not heard from you in a few days. Do you have any update on this post? I want to make sure you are setup for success for your project, but if I do not hear from you I will close this thread. Feel free to post here or on a new E2E post to continue the conversation. Thank you.
If this post answers your question, please indicate so by marking this thread as resolved. Thank you.
Regards,
Michael P.
Applications Engineer
Texas Instruments