This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

univesity project idea on 'Energy Harvesting'

Hi every one!!!

For my final year project, i have decided to implement a energy harvesting application. As to point out the uniquness of my project i also have decided to  use multiple sources to harvest energy in the same application. With some threshold level, the microcontroller will decide which are to be connected with the load. Though this has been the idea, it is hard to figure out in which kind of application i should use the above mentioned system.  

For example using sources such as heat & wind in a motor bicycle. But where to make use this energy is the problem i'm currently working on. As i have seen in the internet, EH wireless sensors are also a very famous topic these days. So please be kind enough to suggest me a appropriate application to my system, and i urge every one to assist me with the  project as it further evolves.

Thanking you in advance,

indunil