Hello
I am working on a application where there is master slave architecture, the master devices and the slave devices are connect by a 50m long cable (2core power +2core signals). The master device provides power to the slave devices. Each switch in the TPS2561 will be connected to a single slave.
1. Can the TPS2561 be used in such a application, to enable / disable power and also the limit power to the slave devices?
2. What kind of minimum protections are recommended in such a application to protect the TPS2561?
3. If the TPS2561 is not the right solution can you recommend any other option? (Electrical requirements are as those met by the TPS2561)
I need to make this a robust and high reliability solution as this will be safety critical in a industrial environment.