Hi All,
I have a design problem here. I am trying to use TPS63010 to get 4.2V @ 2A output. It should be alright if my input voltage is 5V based on figure 1 of the datasheet.
However, the device can be Li-Po battery (nom 3.7V) operated. Based on the chart, I will be getting about 1.5A, not good enough.
Is there a workaround?