Other Parts Discussed in Thread: TPS1HA08-Q1, TPS1HB08-Q1
Dear Sir, Madam,
I am actually using the TPS27S100 to control the load. We are not usind with a Microcontroller but mor as a E-Fuse to limit the current. Our operating current is at 3.5A and we have set the limit at 4A. It is actuallly working, but at 3,5A the boardd becomes too hot. We have checked again and seen that the RDSon is too high. About 100mR. Is there no better replacement with higher current and same pinning? so may be 6A or more wihtout changing our layout. What can you suggest ? or some with very low RDSon, sodass we can try on the same board
Thank you in Advance.
BR
Gilbert