This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ28Z610: removable battery system problem

Part Number: BQ28Z610
Other Parts Discussed in Thread: BQSTUDIO

Hi,
I want to ask question about the removable battery system in BQStudio with bq28z610. 

I use Li-Ion Battery NCR18650 (3400mAh) 2 Cell configuration.  Does it need to be woken up using WAKE switch, in this case shorting Cell 2 pin and PACK+ pin? If do so can you tell why? (according to the EVM schematic)

Is there any solution if batteries are replaced, no need to wake up the system again using 1k ohm shorting these 2 pins (PACK+ and cell 2) ?

Thanks in advance

Regards

Aji