This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Buck converter relationship between Efficiency and Fsw, Inductor

Other Parts Discussed in Thread: LMR23630-Q1

Hi all,

I want to ask about the how efficiency and fsw, efficiency and Inductor are related on the buck converter.

1. Can efficiency can be increased when I change the fsw or Inductance?

2. I calculated based on the datasheet, I could get the minimum Inductance, Lmin, is 3uH. If I use 6uH inductor(all of other condition like DCR are same with 3uH inductor), what can be technical bad effect(except cost and layout size)?

Thank you