This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can't identify Chemistry ID

Other Parts Discussed in Thread: BQEVSW

 

Hi
I tried to identify Chemistry ID using the latest software bqEVSW 0.9.65. Unfortunately, after several hours of communication problems occured after the SMBus. Repeated the process of identifying a few times already. I noticed that the batteries where discharged to the threshold 2500mV causing disconnection Battery Protection and probably by a communication error occured. Could I ask for identification of Chemistry ID on the basis of this log, or help in circumventing the problem.

Best Regards

Wojtek

 

 

4375.Chem.log

  • bqEASY needs 4 OCV data points to do the chemistry matching. Looking at the log file, the last set of data point was corrupted and so the software failed to run the analysis.

    bqEASY will discharge the battery to your min cell voltage level set at step 2A. What is your min cell voltage level set to? 2.5V? Are you using LiFePO4? You will need to raise the min cell voltage level a bit higher, we need to maintain communication in order to log the last OCV data point.

  • HI!

    I used Lithium Polymer battery.

    Please see our project file, where you will see the parameter.

    2C_Dsg_Params.Min_Dsg_Cell_Vltg=2850

    bqEVSW  does't  stop discharge battery on this level.

    [Device]
    Type=0750
    Version=0160
    DFI Filname=C:\Program Files\Texas Instruments\bq Evaluation Software\Plugins\Device Defaults\bq20z75_1_60.dfi
    [Setup]
    1A_Proj_Name.Project_Name=9300
    1B_Load_DFI_File.DFI_Filename=C:\Program Files\Texas Instruments\bq Evaluation Software\Plugins\Device Defaults\bq20z75_1_60.dfi
    [Project]
    Name=9300
    [Configuration]
    2A_Cell_Char.Num_Series_Cells=2
    2A_Cell_Char.Num_Parallel_Cells=1
    2A_Cell_Char.Nom_Cell_Capacity=9300
    2A_Cell_Char.Min_Cell_Vltg=2750
    2H_Misc_Info.Is_Sys_Pres_Used?=True
    2H_Misc_Info.CurrentSenseResistor=10
    2H_Misc_Info.ThermistorConfig=2
    2H_Misc_Info.Number_LEDs_Code=0
    2H_Misc_Info.Mfr_Name=roki
    2B_Chg_Params.Max_Chg_Cell_Vltg=4200
    2B_Chg_Params.Min_Chg_Temperature=0
    2B_Chg_Params.Max_Chg_Temperature=70
    2B_Chg_Params.Chg_FET_Short_Threshold=25
    2B_Chg_Params.Precharge_FET_Mode=1
    2C_Dsg_Params.Min_Dsg_Cell_Vltg=2850
    2C_Dsg_Params.Max_Dsg_Temperature=70
    2C_Dsg_Params.Max_Steady_Dsg_Current=3500
    2C_Dsg_Params.Peak_Dsg_Current=6500
    2C_Dsg_Params.Dsg_FET_Short_Threshold=25
    2D_Reserve_Capacity.Capacity=1
    2D_Reserve_Capacity.Capacity_Units_mAh?=True
    2E_Load_Characteristic.Is_Constant_Current?=False
    2F_Secondary_Vltg_Protector.Is_Used_With_PFIN?=True
    2G_Rem_Capacity_Method.Is_Constant_Load?=True
    [Completion]
    2A=False
    4A=True
    4B=True
    2H=False
    3F=True
    4C=False
    2B=False
    2C=False
    2D=False
    2E=False
    2F=False
    2G=False
    3A=False
    3B=False
    3C=False
    3D=False
    3E=False
    5A=False
    1B=False
    5B=False
    5C=False
    1A=False
    

    Earlier I had set the level of 3000mV and it didn't work.

    Please give me a link to the latest Mathcad™ Chemistry Selection Tool or help me as soon as posible.

    Regards

    Wojtek

  • HI!

    Do you have any news regarding my question?

    Regards

    Wojtek

  • hi,

    when you tried the chemical ID ; did you disconnect the protection IC of your battery ?

    To do the chemical identification, you must work on the cell and not on the battery.

  • I have not seen that problem before. The only thing I can think of is that voltage read by the IC is way off from what the actual voltage is? Have you calibrate the board before running chemistry selection test?

    You can find the z75 product web page (http://focus.ti.com/docs/prod/folders/print/bq20z75.html), go to the Tools & Software section. You will find the mathcad tool download link there.

  • Victorien,

    It's not necessary to disable the protection while running chemistry selection. You will discharge the battery to the min discharge voltage, which is still above your safety threshold.

    When you run the chemistry selection, you have to use the EVM or your own pcb. So you'll need a battery pack to power up your board. (Unless you're working on a single-cell gas gauge, then you'll be working on a cell)