This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ20Z95: BQ20Z95

Part Number: BQ20Z95


Hi,

The Battery which we i am using consist of BQ20Z95 Fuel Gauge IC.In this I can able to read the battery parameters such as voltage ,current,capacity etc.In This i could not able to get the CSV file(Battery Parameter programmed file) from the software.I need to know the battery inbuilt parameters which is set on the battery pack.

Kindly suggest some way to extract the file to read the battery parameters.The Bq screen for your reference.

So that it will be easy to get the Charge termination current,Precharge current of the battery

It is easy to extract the Battery CSV file from the BQ40z50r1 Fuel gauge IC. Likewise suggest the way to read the battery parameters fully.

Thanks in Advance.

Regards

ANANDAN

  • Hello Anandan,

    You can export the .gg file from bqEvaluation software using the file->export function. I think there was a problem with your image upload but I believe this is the configuration file you're talking about.

    Sincerely,

    Wyatt Keller