Hello, I need advice for a pre-regulator design, I don't have much experience in the field, so I'll try to explain my design.
I'm working in a modular design with nodes communicated by CAN protocol, some of the nodes are used to drive power loads like actuators.
My design includes a battery power source of 24V wich will power the actuators, I used for this the DRV8701EVM reference design, but I changed it to replace the micro-usb with an 5V input and CAN protocol.
So now in the board, I have a voltage regulator to convert 5V to 3,3V to power the microcontroller and low power electronics.
I need help to find a way to manage the power source, I need a design to get 5V from 24V battery and I don't know exactly where to start. And what about the battery? should I connect it directly to power the actuators? until now I've been using a laboratory power supply
I would appreciate any help, please help me.