This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2660: TVS Selection

Part Number: TPS2660


Hi,

My customer is evaluating the TPS2660 for an up to 60V rail, and they would like to understand how to size the TVS since abs max of the part is 62V. If they select a 55V or 60V TVS, would the device be able to handle the transient spike? They are looking at 60V TVS with 70V breakdown and 96V clamping which seems too high.

Is there a TVS you would recommend? I don't think reverse polarity is a strict requirement for this system, so feel free to suggest unidirectional if it is the only option.

Thanks,

Antonio