This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24050: Battery is not charging

Part Number: BQ24050


I want to charge the Li-ion battery of 35 mAh and selected the BQ24050.

But now I am  testing on my hardware and seems not working.

It means it is not charging battery and tested with ammeter in series with battery.

Also when battery removed and measured the charger output voltage, it shows 0.38 volt. Here I am expecting 3.7V as connected 237k resistor on TS pin as per datasheet.

1uF capacitor is missing at output side, but it has been taken by 10uF capacitor of 3V LDO.

I also tried to put 1uF capacitor at the BQ24050 output pin, but no success.

We have also tried to short the D+ and D- signal, but no success.

Kindly go through the below schematic and let us know if any mistake or any suggestion to work the borad.