Part Number: TPS54561EVM-555
Hi,
The Datasheet specifies maximum (Abs Max) of 8.4V and On the EVK input range is from 7-60V.
Resistor divider network is been used to set the Minimum operating Voltage.
But At 60V max, EN reads a voltage of 10.5 which is deviating from the datasheet specs Is that okay?
TPS54561EVM-555 Schematic Figure 2.
Thank you.