This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Recommendation for the Li-Ion battery charging chipset

Hello,

I am designing a asset tracking device and I m using 2 of the Sony US18650VTC6 batteries which are 3000mAh capacities each and are Li-Ion batteries. Can you recommend me a appropriate chipset that can be used to charge these batteries. 

Thank you,

Kind regards,

Harsha B R Rao

  • Hi Harsha,

    Are these batteries in series (2S1P) or parallel (1S2P)?  Do you have a host processor/controller to provide I2C communication to the charger or do you need standalone (resistor configurable) charger?  What is you input power source voltage and current?

    Regards,

    Jeff