Other Parts Discussed in Thread: UCC28180, UCC256403, TIDA-010081, UCD3138
Hi Team,
customer has 1kW AC/DC PFC+LLC requirement.
1. I see we have reference using UCC28180+UCC256403/4, can it achieve 0.3W Pin, 0.1W Pout, 0.48W Pin, 0.24W Pout?
I see UCC25640x has burst mode but UCC28180 doesn't have.
2. Is there PFC controller support burst and CCM, and 1kW application?
From website, I do not see it.
3. Is there discrete circuit that can achieve PG function? customer need power good signal before secondary side fully ramp up.
BRs
Given